2022-09-10 09:48 AM
i bought a stm32vldiscovery board from digikeys turkey distrubitor. my computer sees it but stlinkupgrade tells me it is not supported. is there a way to fix this or did i just bought a chunk of glorified useless silicon?
2022-09-12 03:12 AM
Hi @ozan yalçın and welcome to the Community 🙂,
If you refer to RN0093, Known problems and limitations section you can conclude that the ST-LINK (V1) boards are not supported on the Linux® and macOS® operating systems. Only ST-LINK/V2, ST-LINK/V2-1, and STLINK-V3 boards can be updated from these operating systems.
Maybe this discussion can help you to use the STM32VLDiscovery.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-09-12 04:05 AM
Try out openOCD, i use it with my raspi and it works like a charm https://openocd.org/