cancel
Showing results for 
Search instead for 
Did you mean: 

How do I drive the Nucleo_F722ZE board with the STLINK board removed?

chulhoolim-nnftech
Associate III

Hi, everyone.

I cut the stlink board from my Nucleo-F722ZE board.

And I supplied 5V power through E5V of CN11 And JP3 was set to E5V.

I confirmed that the PWR LED was on.

But the embedded program did not run.

I confirmed that this Nucleo-F722ZE board receives MCO input from the STlink board. But now there is no stlink board on my Nucleo.

So, I decided to use the HSI clock rather than the HSE clock.

I set "HSE not used" according to the manual.

 

- SB148 and SB163 ON

-SB112 and SB149(MCO) OFF

-SB8 and SB9 removed

 

And  I enabled HSI in cubeIDE's clock setting.

chulhoolimnnftech_0-1725608565996.png

chulhoolimnnftech_1-1725608601626.png

 

My embedded program on my nucleo runs. But it stops at HAL_Delay().

What part is the problem?

Is the way I did it correct?

12 REPLIES 12

Hi, again.

I did "HSE on-board oscillator from X3 crystal (not provided)" on um1974-stm32.

But stlink doesn't recognize my board. Why?

chulhoolimnnftech_0-1725615415940.png

chulhoolimnnftech_1-1725615434147.png

HSE on-board oscillator from X3 crystal (not provided)

– SB148 and SB163 OFF
– SB8 and SB9 ON
– C37 and C38 soldered with 4.3 pF capacitors
– SB112 and SB149 OFF


@chulhoolim-nnftech wrote:

But stlink doesn't recognize my board. Why?

 


This is another issue. I suggest you to open a new thread.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.