2023-01-30 01:36 AM
please share the link to download the hardware schematic for board NUCLEO=F767ZI
Solved! Go to Solution.
2023-01-30 01:45 AM
Hi @S.sin.1 and welcome to STCommunity ;
You can download the schematic for NUCLEO-F767ZI board from the CAD resources.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-30 01:45 AM
Hi @S.sin.1 and welcome to STCommunity ;
You can download the schematic for NUCLEO-F767ZI board from the CAD resources.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-30 01:54 AM
2023-01-30 02:35 AM
Hello @S.sin.1 ,
The STM32F103CBT6 is another MCU other than the core MCU, which is STM32F767ZI.
The STM32F103CBT6 is an integrated MCU existed in Nucleo-F767ZI and related to ST-Link.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-30 04:15 AM
Hi,
Page 3 in the schematics belongs to the ST-Link part.
The remaining pages are related to the STM32F767 schematics.