2022-03-01 02:07 PM
the error:
STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0-RC1
-------------------------------------------------------------------
ST-Link Server is running on port : 7184
ST-LINK SN : 30FF6F065647373734141043
ST-LINK FW : V2J37S7
Board : --
Voltage : 2.95V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a24696.srec
File : ST-LINK_GDB_server_a24696.srec
Size : 2704 Bytes
Address : 0x08100000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 8
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.2.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.6.0.202101291314\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
2022-03-01 02:09 PM
this is whats happens before i see an error, it is stuck there for 5 min and then error pops up
2022-03-02 12:54 AM
Hello,
2022-03-02 01:06 PM
hi
sofLit,
i check every thing, but its not the power or the connection. i solved it by connecting the ST-Link VCC to the board VCC. when i connect the external power then i am having the problem.