cancel
Showing results for 
Search instead for 
Did you mean: 

hello I'm trying to use SVW on STM32H735g-dk, but it doesn't work. It's not even specified in the manual. Is there anything to set on the PCB?

moon1003
Associate III
 
5 REPLIES 5

Which Version of the PCB ?

MB1520-B02 looks to have SWO connectivity to the ST-LINK/V3

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

MB1520-B02-H735I Board is in use.

Is it possible to use SWV directly without setting on the board?

I'm trying to read the manual, but I've done all the settings

>>Done all the settings

Sorry you'll need to be more precise.

What's the SWCLK, and do you have the ratios correct?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I tried setting it to low speed and automatic as shown below.

All settings are attached.

0693W00000Nq10IQAR.png 

0693W00000Nq10NQAR.png 

0693W00000Nq10SQAR.png 

0693W00000Nq0zQQAR.png 

0693W00000Nq116QAB.png

When debugging, sometimes the following error window appears

0693W00000Nq13CQAR.png