cancel
Showing results for 
Search instead for 
Did you mean: 

SMPS power Regulator is not being set in STM32U575.

nilesh-dryad
Associate III

I am trying to set up SMPS power Regulator for low power operation. I am using Nucleo-U575ZI-Q board. I set the bit in CR3 register but bit in SVMSR is not being set.

Do anyone have idea what can be wrong? Is there something that I am missing?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Bruno_ST
ST Employee

Hello @nilesh-dryad​ 

Did you enable the RCC->AHB3ENR PWREN (bit 2) before poking the PWR->CR3 REGSEL to 1 ?

Then yes, you you see switch the SVMSR toggling to 1.

BR,

Bruno

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

nilesh-dryad
Associate III

@Bruno_ST​ 

Thank you for your quick reply.

I am using the example from STM32CubeIDE for Nucleo-U575 without any change. Am I supposed to change anything in example?

BR,

Nilesh Vora

Typically the PWR peripheral is enabled via HAL_Init() and its call to HAL_MspInit() stm32u5xx_hal_msp.c

The SMPS settings via SystemPower_Config()

See example

STM32Cube_FW_U5_V1.1.0\Projects\NUCLEO-U575ZI-Q\Examples\CRC\CRC_Example\Src\main.c

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I checked Hal_Init function, it is set. Do I need to set any jumper or solder bridge on Nucleo board? I checked the user manual of the nucleo board. I didn't find anything related to SMPS.

It is enabled. I checked it. I don't understand why the sample examples are not working on nucleo board.

I also checked TX_LOWPOWER example, it is also not working. Power consumption is always around 60ma. Tickless idle also does not seem to work. I didn't try all the examples.

Bruno_ST
ST Employee

Examples should work straight away without any change on the board.

For Tx_LowPower, LED_GREEN toggles every 500ms for 5 seconds each time user press the user button (consumption ~4/5uA). Something looks wrong on your Nucleo MB1449 board. Consumption under reset ~550uA (black button keep pressed and IDD measure on pin 2 of JP5 means on VDD_MCU side)

Bruno

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

nilesh-dryad
Associate III

Strange. I have 3 Nuclen board with me. I tried on two. I didn't work but today I opened the 3rd one and the examples worked on the 3rd one. So the SMPS regulator worked on 3rd one.

Bruno_ST
ST Employee

Yes, strange... as the board is tested in production...

When you say the 2 first boards are not working, the issue is only on SMPS that doesn't start on the board ?

Is the on-board SMPS on JP4 @1.8V ok ?

60mA is so high ! The U575 doesn't consumes so much on LDO @160MHz at 25°C.... (cf datasheet)

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

nilesh-dryad
Associate III

If you switch to LDO on those two boards then it works fine.

One more question: Do I need to switch to 1.8V if I enable SMPS power regulator?