2023-02-14 5:39 AM
I saw the problem when I use them for a basic LED Blink code. The Code got stuck in a while loop in SystemClock_Config() function. I tried lots of things.
My __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1) will not return to SystemClock_Config(). I found that PWR->CSR1:ACTVOSRDY bit is staying at 0. I could not find any solution.
In my hardware the power supply was SMPS supply as its default. I did not change anything on hardware.
The same error occurred even if I use the example codes from CubeIDE. This time, the code got stuck in a similar structure but in SystemClock_Config() also here.
More interestingly, both my 2 of the STM32H745I-DISCO boards have the same problem.
How can I fix the problem, I am open to any suggestions.
2023-02-16 2:05 AM
Hello @Furkan Yüksel ,
You can refer to the following example provided under the H7 Firmware Package:
Otherwise, make sure you are not in the simulator debugger mode and take a look at this video, it could help you.
BeST Regards,
Walid
2023-02-16 6:04 AM
The problem in GPIO_EXTI in my board is that in the line 138 in main.c (for CM7) the code has
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) { }
The code got stuck in here, similar to my other projects either that I created or the examples that I used. They are all got stuck in the SystemClock_Config(), the stuck point changes only
2023-02-16 6:36 AM
Anything remarkable about how these boards are powered?
Modified, got other shield / boards plugged in?
Shouldn't have an LDO / SMPS issue as the code specifically targets the board.
2023-02-16 10:22 PM
I use CN3 -> VIN to power the board. I did necessary manipulations to properly power the board.(JP8 -> E5V jumper is used)
On the board the LD4 LED is indicating whole board powered or not. I do a double-check on it.
However, although I tried the other power selections like powering on STLink's USB, the behavior did not changed.
I use only the board. I did not modify it. Therefore the board is in default state (SMPS). I double-checked it by looking the components that are placed in the board and not placed in the board. I am sure that board was configured as SMPS.
Therefore, I don't think that the problem is a LDO/SMPS issue. There could be problems in the SPMS configuration components, but my second board has the same behavior which makes me confused.