2024-12-29 08:54 AM
Hi,
I'm trying to get started with the STM32 NUCLEO-H7S3L8 board to create a USB HS device. I am new to the boot/application split development (also to trustzone) and don't know where to find the right resources to get started. I have tried using the STM32CubeIDE examples importer but keep receiving "failed to copy error" which I don't know how to debug. I have also tried loading the project from the git repo, I can compile and run the boot project but know how to properly setup the application project to run as well.
I would really appreciate some pointers on where to find the information to get the CDC_Standalone example running and how to develop with the boot and application.
Apologies I can't be more specific, I seem a little out of my depth and don't know where to start!
2024-12-30 02:18 AM
Hello @Linduri, welcome to ST Community,
Here are some solid resources you can start from to understand the boot/application split development;
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-30 10:37 AM
In addition to the links above, here you can help and support with your STM32 project.