cancel
Showing results for 
Search instead for 
Did you mean: 

Error in UM2408 on LD1 connection

TDK
Guru

There is an error in UM2408 regarding the connections for LD1.

In section "6.6 LEDs", it currently reads:

User LD1: a green user LED is connected to the STM32H7 I/O PB0 (SB39 ON and SB47

OFF) or PA5 (SB65 ON and SB54 OFF) corresponding to the ST Zio D13.

It should read:

User LD1: a green user LED is connected to the STM32H7 I/O PB0 (SB54 ON and SB65

OFF) or PA5 (SB65 ON and SB54 OFF) corresponding to the ST Zio D13.

https://www.st.com/resource/en/user_manual/dm00499171.pdf

If you feel a post has answered your question, please click "Accept as Solution".
1 REPLY 1
Imen.D
ST Employee

Hello @TDK​ ,

Thank you for reporting this error. We will correct this in the next release of UM2408.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen