2022-11-06 11:02 AM
Hello @ST_community,
I am Trying to program STM32-H7A3ZI-Q Nucleo board.
I couldn't debug the board attached the images for reference. Also Attached the log file for reference. Please let me know how to debug.
Thanks,
Solved! Go to Solution.
2022-11-06 11:19 AM
Suggests the MCU is non-responsive.
Did you program it previously?
Does it work with STM32 Cube Programmer as a stand-alone application?
If you have the LDO/SMPS settings wrong you can block access to the STM32.
The trick then is to solder a jumper between BOOT0 (BT0) and VDD.
With BOOT0 HIGH remove ALL power and USB
Reapply power/connections.
Attempt to access via STM32 Cube Programmer.
If that succeeds, ERASE your code from the part.
Fix your code.
2022-11-06 11:19 AM
Suggests the MCU is non-responsive.
Did you program it previously?
Does it work with STM32 Cube Programmer as a stand-alone application?
If you have the LDO/SMPS settings wrong you can block access to the STM32.
The trick then is to solder a jumper between BOOT0 (BT0) and VDD.
With BOOT0 HIGH remove ALL power and USB
Reapply power/connections.
Attempt to access via STM32 Cube Programmer.
If that succeeds, ERASE your code from the part.
Fix your code.
2022-11-06 6:54 PM
Hey Clive, should the board use copper pads for tweezer boot short to bootloader, or slide switch for a more permanent solution? Say user developping his own bootloader or other possible cases?
2022-11-07 3:16 AM
Thank you, sir.
It works
2022-11-07 6:59 AM
After having to do this more than once, I find the following to be a workable solution, along with the spare jumper(s) ST conveniently parked on the back of the board. People should do whatever works for them..