cancel
Showing results for 
Search instead for 
Did you mean: 

Error in final launch sequence

Hardik02
Associate II

Certainly! Here’s a revised version of your post:


Title: Trouble Flashing p2pServer_Ext Application on Nucleo WBA52CG Board


Hello,

I am attempting to run a p2pServer_Ext sample application on my Nucleo WBA52CG board. Currently, I have a heart rate sensor application running on the same board. However, when I try to flash the new p2pServer_Ext application, I encounter an error. called Error in final launch sequence

I have two identical boards, one of which runs the p2pClient sample application. Interestingly, I can successfully flash the same p2pServer_Ext application on the other board using the same laptop and STM32Cube IDE software.

What could be the possible reason for this issue, and what is the solution? My supervisor suggested that electrostatic discharge (ESD) during handling might be the cause, but the existing heart rate application works flawlessly. The problem seems to be specific to flashing new software.

Any insights or recommendations would be greatly appreciated.

 

0 REPLIES 0