2021-01-11 5:07 AM
Hello Forum,
recently I bought me a new ST-Link/V2 to program and debug a STM32L4. I tried to connect the programmer with the MCU, but it didn't work. Now I tried it with a different programmer and I could establish a connection to the STM32L4. After that I tried to connect the new programmer with a STM32G0 and this also works.
Version of new programmer: ST-Link/V2 A2020 03
Version of old programmer: ST-Link/V2 B2017 15
Both programmers have the same Firmware Version.
Could anyone please tell me where the error is?
Kind regards
Eric
Solved! Go to Solution.
2021-02-10 10:59 PM
Hello,
thank you for your answers. But a few weeks ago I talked to an ST employee and showed him the schematic of the STML4. I forgot the 100 nF capacitor at Reset...
Kind regards
Eric
2021-02-10 2:33 PM
Carefully and double check all connections, USB cables and USB ports, I do not think there is a real functional difference in both versions.
2021-02-10 2:55 PM
Are these authentic or clones?
Watch that you're powering pins 1 or 2 with VTarget so as to power the buffers.
2021-02-10 4:39 PM
"Are these authentic or clones?"
+1
If you've got cheap clones like this from ebay or the like:
beware that there are at least two different pinouts on otherwise identical-looking products!
EDIT
Here you go:
Click the image to enlarge - Look carefully at the two pinouts!
2021-02-10 10:59 PM
Hello,
thank you for your answers. But a few weeks ago I talked to an ST employee and showed him the schematic of the STML4. I forgot the 100 nF capacitor at Reset...
Kind regards
Eric
2021-02-11 1:21 AM
Thanks for the update - it would have been helpful if you had said that earlier!
So that the forum shows the issue as solved, please 'Select as Best' on your answer:
Then the 'Answered' flag will be shown in the forum listings: