2024-03-06 12:59 AM - edited 2024-07-22 2:47 AM
2024-03-06 5:29 AM
Hello @Bonnie ,
You can refer to the Getting started with STM32L0xx hardware development in section in section 6-Reference design
where you can find some useful details about the implementation of the STM32L0 series MCUs.
You can also inspire from NUCLEO-L073RZ in this link .
BR
2024-03-06 6:13 AM
Start by reviewing the Data Sheet, paying special attention to power, capacitors, BOOTx and NRST. Make sure to escape a means of programming/debugging via SWDIO/SWCLK, and understand the system loader via AN2606
Most of ST's boards have schematics, and these can be found under the "CAD Resources" tab on the respective product pages.
2024-03-06 6:17 AM
@Bonnie wrote:I'm new to designing with STM32 chips
Are you familiar with designing for other microcontrollers? Much of it is common...
2024-03-06 6:19 AM
@Tesla DeLorean wrote:Make sure to escape a means of programming/debugging via SWDIO/SWCLK
Absolutely!
@Bonnie Best to also include NRST - that can get you out of some holes where the debugger can't access the Target...