2020-12-04 10:49 PM
Hello. I don't know exactly what the IDE needs, but it doesn't seem to see the St link server, but at the same time says that it is installed. When you press the Debug or Run button, a window appears with the inscription "ST-Link Server is required to launch the debug session. Please download in on www.st.com".I tried versions 1.5, 1.4 and as far as I remember 1.1. I wanted to try other versions, but the download was constantly interrupted. Is it just me or everyone? It looks like the site needs mirrors.
Separately downloaded St-link-server 2.0.2. At the time of installation, the answer was
"sudo ./st-stlink-server.2.0.2-1-linux-amd64.install.sh
[sudo] пароль дл�? gadzhi:
Creating directory makeself_dir_o9t3i4
Verifying archive integrity... All good.
Uncompressing STM STLink-Server installer 100%
STMicroelectronics Software License Agreement
<License...>
License accepted.
stlink-server v2.0.2 (2020-10-13-14:11) installation started.
Already installed version is newer or equal: �?трока 64:
NOT downgrading. Aborting stlink-server installation.
Error installing stlink-server".
I also tried to install the server through Help> Install New Software ... Answer:
"Cannot complete the request. See the error log for details.
"STM32CubeIDE MCU External Tools ST-LINK GDB Server" will be ignored because a newer version is already installed.
"STM32CubeIDE MCU External Tools SEGGER J-Link GDB server" will be ignored because a newer version is already installed.
"STM32CubeIDE MCU External Tools ST-LINK Server" will be ignored because a newer version is already installed."My main system is Manjaro Linux (system updated). Everything works well on Windows 10. I tried to program two boards and there were no problems.
I am newbie, don't kick me hard and please explain in detail.
I am looking for a solution in 4 or 5 days. I was looking for two of them incorrectly - why the IDE does not see stlink, but it turned out that it does not see not stlink, but stlink server.
I searched a lot and everywhere, asked in many Telegram chat channels. I came here last, because I prefer to look for the answer myself and because I don't know English and this is Google Translator. Therefore, I'm sorry if you don't understand something in this text.
2021-01-21 01:19 AM
Thanks for these steps!
To get your steps to work on my Windows 10 machine, I had to also uninstall "STMicroelectronics stlink-server" through Apps & features. Otherwise the installer would fail.
2021-01-21 03:43 AM
have the same question.
did not find a way to uninstall stlink-server on linux.
did not find any thing like `st link server` from `apt` command or from CubeIde.
but tell me already installed new version when I tried to install.
2021-02-24 04:14 AM
Проблему решил на Ubuntu 20.04:
1) Удалил STM32CubeIDE
2) У�?тановил ST-Link Server
3) Заново у�?тановил STM32CubeIDE (ver 1.4.0)
2021-03-04 09:39 AM
2 ways:
2021-06-19 07:14 AM
tried this it really helped me. thank you.
2022-02-18 03:03 AM
Hi, I had the same problem with Windows 10. I was using IDE version 1.8.0. Here is how I solved it.
2023-04-25 09:53 AM
Hi,
i am facing the same problem but after installation st link server the problem solved.