2020-12-04 10:49 PM
Hello. I don't know exactly what the IDE needs, but it doesn't seem to see the St link server, but at the same time says that it is installed. When you press the Debug or Run button, a window appears with the inscription "ST-Link Server is required to launch the debug session. Please download in on www.st.com".I tried versions 1.5, 1.4 and as far as I remember 1.1. I wanted to try other versions, but the download was constantly interrupted. Is it just me or everyone? It looks like the site needs mirrors.
Separately downloaded St-link-server 2.0.2. At the time of installation, the answer was
"sudo ./st-stlink-server.2.0.2-1-linux-amd64.install.sh
[sudo] пароль дл�? gadzhi:
Creating directory makeself_dir_o9t3i4
Verifying archive integrity... All good.
Uncompressing STM STLink-Server installer 100%
STMicroelectronics Software License Agreement
<License...>
License accepted.
stlink-server v2.0.2 (2020-10-13-14:11) installation started.
Already installed version is newer or equal: �?трока 64:
NOT downgrading. Aborting stlink-server installation.
Error installing stlink-server".
I also tried to install the server through Help> Install New Software ... Answer:
"Cannot complete the request. See the error log for details.
"STM32CubeIDE MCU External Tools ST-LINK GDB Server" will be ignored because a newer version is already installed.
"STM32CubeIDE MCU External Tools SEGGER J-Link GDB server" will be ignored because a newer version is already installed.
"STM32CubeIDE MCU External Tools ST-LINK Server" will be ignored because a newer version is already installed."My main system is Manjaro Linux (system updated). Everything works well on Windows 10. I tried to program two boards and there were no problems.
I am newbie, don't kick me hard and please explain in detail.
I am looking for a solution in 4 or 5 days. I was looking for two of them incorrectly - why the IDE does not see stlink, but it turned out that it does not see not stlink, but stlink server.
I searched a lot and everywhere, asked in many Telegram chat channels. I came here last, because I prefer to look for the answer myself and because I don't know English and this is Google Translator. Therefore, I'm sorry if you don't understand something in this text.
2021-01-08 4:45 AM
Hi Gadzi! I also just encountered the same problem on Windows 10. Very strange that it suddenly stopped working. Being a newbie unfortunately I cannot help either. But I am trying now to see what potentially could go wrong.
2021-01-09 10:05 AM
Hi i was helped by installing en.st-link-server and additional packages in linux:
sudo apt-get install libncurses5 libgpm2:i386 libncurses5:i386
and select sudo usermod -a -G dialout user_name, then reboot the system, after that everything is determined
(mxlinux distribution)
2021-01-11 7:09 PM
Hi
I met the same problem on Ubuntu 20.04, CubeIde 1.5.1
tried to install st-link server from st.com website or `install new software` in CubeIde, do not work
tried SSerj.1's method, do not work
need help plz!
2021-01-13 8:28 AM
I installed the same versions of packages that you specified, and also gave permission to the user, but nothing has changed.
This is the default debugger configuration
2021-01-14 8:28 AM
2021-01-14 8:30 AM
2021-01-14 8:30 AM
2021-01-15 2:17 PM
The following solved the problem for me (Windows 10, CubeIde 1.5.1):
2021-01-16 7:56 AM
In windows 10 everything works for me. What's the path of stlink-server in linux?