2019-04-02 4:26 AM
The product page for STLINK-V3SET lists the following:
Multi-path bridge USB to SPI/UART/I2C/CAN/GPIOs
I can see in the STM32CubeProgrammer CLI that use can use the SPI/I2C/CAN/UART functions. But can you control the state of the GPIO 0-3 pins in some way?
2023-03-13 2:45 AM
It would be greatly appreciated if someone could assist with the following matter: I have also been unable to find any references or guides describing the process for controlling the GPIOs of the ST-link V3 using the CLI interface.
Is it even possible?
Thanks