2025-02-07 08:55 AM
Dear community,
I have a nucleo board NUCLEO-G071RB and I would like to use the Build-In USB in the STM32G071, is there a shield or an expansion board compatible with this nucleo board, that allow me to access to the USB
Thank you in advance.
Best regards
Bassem
Solved! Go to Solution.
2025-02-07 09:17 AM - edited 2025-02-07 09:21 AM
Asslema @Bassem
I think the content of this webpage: STM32 solutions for USB Type-C and Power Delivery - STMicroelectronics should help you. there is a description for the x-nucleo-snk1m1, x-nucleo-drp1m1 and x-nucleo-src1m1 also, you can find the X-CUBE-TCPP
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-07 09:04 AM
This is one of the biggest dropped balls on the part of the NUCLEO expansion teams part. Hopefully someone else has a GOOD suggestion that isn't just flying wires. The closest I've found is NUCLEO2USB:
https://github.com/dmitrystu/Nucleo2USB
2025-02-07 09:12 AM - edited 2025-02-07 09:13 AM
Actually there are at least two ST boards with USB connectors:
X-NUCLEO-SNK1M1
X-NUCLEO-CCA02M
Newest Nucleo-64 boards (U5xx, C071, H5xx) finally contain the USB connector for target CPU.
2025-02-07 09:17 AM - edited 2025-02-07 09:21 AM
Asslema @Bassem
I think the content of this webpage: STM32 solutions for USB Type-C and Power Delivery - STMicroelectronics should help you. there is a description for the x-nucleo-snk1m1, x-nucleo-drp1m1 and x-nucleo-src1m1 also, you can find the X-CUBE-TCPP
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-07 09:18 AM
For testing, any cheap USB breakout board will do.
Not G0 but C0 with USB 2.0 FS device (crystal-less) and host controller and USB Type-C connector:
hth
KnarfB
2025-02-07 10:08 AM
Thank you guys for the suggested solutions, the solution with STM32C071 looks very promising, but unfortunately the proof of concept that I'm preparing is based on STM32G0, so it looks like the expansion boards X-NUCLEO-SNK1M1
and X-NUCLEO-CCA02M could help and avoid flying wires, so to be more investigated.
2025-02-07 11:35 AM
If your question is answered, please select the answer that have done the job for you as Best answer.
Salem.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.