cancel
Showing results for 
Search instead for 
Did you mean: 

COIN CELL BATTERY

Anu
Associate

Hi,

I am working on STM32F407VGT6 DISCOVERY BOARD , here i want to place a coin cell battery and my doubt is, does the board contain an external super capacitor and where can i design a coin cell battery.......please help me to sort out this problem

3 REPLIES 3
Vincent H
Associate III

Not sure you'll get an answer to this one,

"does the board contain an external super capacitor" is a bit of an oxymoron.

Plus, this board requires a 5V power supply, and as far as I know most coin cell batteries are 1.5 or 3V.

Do you have an EE in your team ?

Maybe @Anu wants to power the RTC and/or backup SRAM from the coin cell, through the VBAT pin... but it's upon him/her to explain what exactly are the requirements.

JW

Ozone
Lead

I think a look at the schematics should reveal the answer - no, there is no super capacitor at the original F4 discovery board.

And it would be useful for adding the coin cell (identifying/checking the pins).

I suppose it is clear to the OP that the board cannot be powered by the coin cell, it is only for RTC/backup RAM.