cancel
Showing results for 
Search instead for 
Did you mean: 

can you open source your STLINK-V3MINIE?

FZhen.3
Associate II

Can you open source your STLINK-V3MINIE?  

All hardware and codes,  

Your design is not easy to use.

13 REPLIES 13
TDK
Guru

ST isn't going to open source ST-Link.

What's hard to use about it? Likely someone can help if you describe what problem you are having.

If you feel a post has answered your question, please click "Accept as Solution".
STTwo-32
ST Employee

Hello @FZhen.3 

As suggested by @TDK , you can ask any question about this product and the community members will try to help. You can also refer to the UM2910 for details about using this product. 

If you have any special needs on this product, you can reach to our sales & marketing teams, to our FAEs or to the online support services.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@STTwo-32  

Screenshot_72.jpg

Thanks for your advice,

Then can you design a new version of STLINK-V3MINIE  like this?

Look at the picture in attachments  

@TDK  

 

Thanks for your advice,

Then can you design a new version of STLINK-V3MINIE  like this?

Look at the picture in attachments  

 

Screenshot_72.jpg

Peter BENSCH
ST Employee

@FZhen.3 What you show in the double-inserted picture is not an open source tool, but an illegally manufactured and incomplete clone of the ST-LINK/V2, with which there are meanwhile massive problems due to its incompatibility. STMicroelectronics does not support such counterfeits, nor does it make any variant of the ST-LINK available as open source - because otherwise we would no longer be able to guarantee compatibility and interoperability.

Regards
/Peter

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@FZhen.3 there's no need to post the same thing twice in two separate replies - everyone can see all posts!

Andrew Neil
Evangelist III

@FZhen.3 wrote:

Can you open source your STLINK-V3MINIE?  


ST has never open-sourced any ST-Link hardware or software - why would they start now?

But there are open-source debug adaptors available; eg,

https://black-magic.org/index.html

https://os.mbed.com/handbook/CMSIS-DAP

https://flirc.tv/products/flirc-jeffprobe?variant=43085036585192

 


@FZhen.3 wrote:

Your design is not easy to use.


Why not? In what way(s), specifically, do you find it "not easy" ?

As the others have said, if you describe the problem(s) then people can probably help you to overcome them...

 

Like, me personally? Yes, I have the skills necessary to do so.

Why not just use a debugger that exists and works well like the STLINK-V3MINIE?

If you feel a post has answered your question, please click "Accept as Solution".

@TDK  

STLINK-V3MINIE  is not convenient to use, Doesn't have a outer casing, It is easy to damage, and the wiring is inconvenient.