Hi there,I want to use a usart port to control EVSPIN32G4 board,start,stop,set motor speed,etc, where can i find those protocol or code,X-CUBE-MCSDK_5.Y.4 version.Thanks。
Hi Sensorless BLDC can't run very well at low speed,I would like to know which STM32 series or which ST motor control workbench version can support HFI,and if support,can it run sensorless bldc motor well at low speed?Or none of them can support HF...
@Peter BENSCH Illegally manufactured, incomplete clone, maybe. But massive problems are not. works very well acctually.I am not support illegally manufactured product , But they really consider issues from the perspective of users!Maybe a large c...
@Andrew Neil Thanks, I‘m using CMSIS-DAP, works well.But STLINK has some unique features, like programming Option Bytes of stm32XX. other debug adaptors can't.