cancel
Showing results for 
Search instead for 
Did you mean: 

CAD resources of NUCLEO-H755ZI-Q Revision D-01

Lupillo_1788
Associate

I'm looking for CAD resources of NUCLEO-H755ZI-Q  board Revision D-01. Currently en the web-page there are for revision C-01.

 

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,

Update, design files for rev D01 should be there:

CAD resources 

View solution in original post

7 REPLIES 7
Rodo
Senior

It could be that there are no changes to the PCB. You could compare the two BOMs and see what the difference is/are. That would take some time though. It would be nice to have a list of Engineering Change Notices (ECNs) on the schematic or elsewhere.

Mike_ST
ST Employee

Hello,

>> It could be that there are no changes to the PCB

If the revision has moved from C to D, that means PCB has been changed. It could be minor (like silkscreen) or not.

I have entered an internal ticket #211945, to see if it can be added.

 

Andrew Neil
Super User

I see both Revision D-01 and C-01:

AndrewNeil_0-1749630920735.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

>> I see both Revision D-01 and C-01:

Maybe I'm wrong, but I understood the request was for "MB1363 Board design project files" and "MB1363 Manufacturing files" which are only for Rev. C, because, as you mentionned, schematics for rev C and D are there.

 

Maybe:  @Lupillo_1788 just said, "CAD resources" - didn't say what "resources", specifically.

But the BoM, Manufacturing, and Design files are all dated after the D01 schematics ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
The altium design files are missing for last revision.

Hello,

Update, design files for rev D01 should be there:

CAD resources