2024-05-11 10:41 PM
Hello people.
I just worked on a audio processing project with am STM32F407 discovery board. And everything went fine.
But now I'm looking to work with a board that allows to connect a usb webcam and stream it to 2 monitors through HDMI (I assume this might work better with an MPU rather than an MCU. Since I need the best processing possible on this project.)
The thing is, I have no idea how to pick the right board for this... I don't want to order a bunch of boards and test one by one. I will rather ask to the community for suggestions.
I'd like to mention I'll need the board to have OTG usb, to use it as a host for storing screenshots.
Thanks.
2024-05-14 2:06 AM
@Lalo91 wrote:I assume this might work better with an MPU rather than an MCU.
Probably.
And, if you're looking for HDMI, probably an SBC rather than a bare MPU.
I'd be looking at something like a Raspberry Pi for this ...
ST's MPU range is here:
https://www.st.com/en/microcontrollers-microprocessors/stm32-arm-cortex-mpus.html
2024-05-14 6:05 AM
Hello, thanks for your reply back...
I can't fall into SBC's once again, and even less if its por commercial. At first, I built this project in an RPi4 and then migrated it to an Nvidia board... I can't explain enough how much I dislike sbc, since now on, I will work on bare mcu/mpu which at the end is the way to go (harder, but it is), and more if its for commercial.
Thanks! I check out the link you provided. I hope to get a "easy" to code board. I wouldn't like to built a library from scratch just you read a webcam and output through hadmi. And actually, not necessarily it needs to be a webcam, I could also look at bare camera modules and connect them directly to gpio.