cancel
Showing results for 
Search instead for 
Did you mean: 

BLE samples hardware configuration

GS2
Senior

Hello, Where can I find hardware configuration for BLE examples in case of development and production? Particular for STM32WB BLE-HID.

1 ACCEPTED SOLUTION

Accepted Solutions

The joystick is available for the Discovery board of the STM32WBA. This application can run only on an STM32WBA discovery. It is not compatible with the NUCLEO-WB55 board.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Hello @GS2 

Can you give more details about your request?

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

For example from BLE_HID_Mouse - how mouse and (the joystick?) should be connected to NUCLEO-WB55 board ?

"Now you can control the mouse pointer by using the joystick direction of the STM32WBA55xx Discovery kit,
selection can be done with a press on the joystick."

The joystick is available for the Discovery board of the STM32WBA. This application can run only on an STM32WBA discovery. It is not compatible with the NUCLEO-WB55 board.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.



As @STTwo-32 said, it is referring to The Joystick which is part of the Discovery kit:

AndrewNeil_0-1719328794486.png

So you don't need to do anything - it's already done for you!

AndrewNeil_1-1719328934178.png

 

To use a Nucleo board, you'd have to replicate all those features of the Discovery kit

 

 


@GS2 wrote:

For example from BLE_HID_Mouse - how mouse and (the joystick?) should be connected 


You don't connect a mouse - it uses the joystick instead of a mouse:

"Now you can control the mouse pointer by using the joystick direction of the STM32WBA55xx Discovery kit, selection can be done with a press on the joystick."