cancel
Showing results for 
Search instead for 
Did you mean: 

B-U585-IOT02A inport BSP project

ElectroManiac
Associate III

Hello forum,

Im trying to build a function based on the BSP example and all the peripheral sensors,
when opening a new project and adding the libraries and drivers from the BSP example, nothing works.
some of the files have missing defines which suppose to come from the autogenerated files of the STM32CubeIDE

what am I doing wrong?
thanks in advance

1 REPLY 1
Florian LR
ST Employee

Hello @ElectroManiac , 

Which libraries did you add ? Do you know what are the missing files/defines ?

Another solution is to open directly the BSP example available under Projects\B-U585I-IOT02A\Examples\BSP in the STM32Cube_FW_U5

Best Regards, 

Florian LR