cancel
Showing results for 
Search instead for 
Did you mean: 

Anyone has a schema of this STM32H750 board?

Pavel A.
Evangelist III

0690X00000AsO4jQAF.jpg

E-bay sellers don't have any docum, even Chinese.

It contains some I2C eeprom and SPI flash - but to which SPI and I2C they are connected?

Also, I've tried to wire up a white ST-LINKv2 dongle to the SWD debuger contacts, but no success. According to this.

No software can see the target.

The board is alive. It has some test firmware from the factory that blinks LEDs and emulates a USB COM port to host. (but the port does not output anything and does not react to input at 9600 or 115200).

-- pa

1 ACCEPTED SOLUTION

Accepted Solutions
MacLaren
Associate III
11 REPLIES 11

https://community.st.com/s/question/0D50X0000BcSqt1SQC/forum-noise-wow-stm32h767-board-available-before-st-released-the-product

Wired up the SWD pins to a stand-alone ST-LINK/V2, no problems here.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MacLaren
Associate III

hope useful

Pavel A.
Evangelist III

Great, thank you

Hello Mr. Avogadro (or still Clive?)

Have you wired the reset and SWO to the debugger tool?

Still cannot get it working...

-- pa

Just wired VCC, GND, SWDIO, SWCLK

0690X00000AsO6zQAF.jpg

(1) Top Left VCC

(8) Right 4th Down GND

(7) Left 4th Down SWDIO

(9) Left 5th Down SWCLK

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Great, it works now. Thank you a lot.

-- pa

Piranha
Chief II

VDDA/VREF+ isn't bypassed with any capacitors! They are not even able of copying reference design.

Buttons also could be debounced...

> Buttons also could be debounced

I"ve pulled the buttons up and down, as Clive advised, They work good enough for me. Will post the Cube file later, for those who cubes))

-- pa

Attached is a Cube file for CubeIDE.

(a minimal version suitable for my project).

-- pa