2024-04-15 09:57 PM
I have tested ST25DV16KC Type 5 NFC Tags in out products using ST25 NFC mobile application.
For automating my testing process using PC based utilities, I am looking for NFC Type 5 card readers which will support your ST25DV16KC IC.
Previously I have used Identiv3700F cards which support only Type 3 NFC Tag, now I can't use that because ST25DV16KC is Type 5 NFC Tag.
Can you suggest any NFC card reader/writer which have GUI or which I can access for automating my stuff?
2024-04-16 08:38 AM
Hi,
ST25R3911B-DISCO or STEVAL-25R3916B can be used to read Type 5 Tags. Those NFC reader boards can be connected to a PC through USB and a GUI is available on st.com. A communication DLL is also available so that you can interface directly with the board. See https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/c-application-for-steval-25r3916ba-using-st25r3916discocomm-dll/td-p/657782
Rgds
BT
2024-04-19 08:07 AM
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.