cancel
Showing results for 
Search instead for 
Did you mean: 

NXP NTAG compatibility with CR95HF

DWann
Associate III

As I understand it, NXP's NTAG family (NTAG 210u, NTAG 21x) are fully compliant NFC Forum Type 2 and ISO/IEC14443 Type A devices, and as such, they should work with the CR95HF. However, these tags have additional features, like an originality signature, that areoutside the scope of the standards. Are these additional features compatible as well, or are they only supported by NXP readers?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

​Hi sir,

According to the NXP specification, even if the command are outside the scope of the standards, this feature should be accessible with the CR95HF if you program the appropriate command with the suggested protocol. The CR95HF will only do the transfer all has to be pre processed by the micro-controller.

Regards

PB

View solution in original post

1 REPLY 1

​Hi sir,

According to the NXP specification, even if the command are outside the scope of the standards, this feature should be accessible with the CR95HF if you program the appropriate command with the suggested protocol. The CR95HF will only do the transfer all has to be pre processed by the micro-controller.

Regards

PB