cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3911B-DISCO using ST25SDK

itsgimbi
Associate II

Hi, I am trying to develop a mobile java application using the ST25R3911B-DISCO and saw that ST offered the ST25SDK to help. When looking deeper into the SDK, I saw that there are some reference implementations using the ST25R3911-DISCO but one of the limitations is that it is only supported in 32-bit configuration. I was wondering why this is as there is a PC GUI that works on Windows 64-bit and if there is a way I can try to edit it to make it compatible with different platforms. 

1 ACCEPTED SOLUTION

Accepted Solutions
Berenice BENVEGUDA
ST Employee
2 REPLIES 2

Hello,

we are working on the development of ST25PC GUI and reader DLL for 64-bit Windows platform. Support of ST25R3911B-DISCO will be included. We plan to deliver this version by beginning of 2024. We will advise you as soon as this version will be available.

Best regards,

NFC Customer support 

Berenice BENVEGUDA
ST Employee

Hello,

See following post, where the 64-bit version has been announced :

https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/is-there-a-64-bit-version-of-st25r3916discocomm-dll/m-p/653505#M10542

Best Regards,

BB