2024-11-14 1:59 AM
Hello!
I am working on integrating ST25R3916B into our product based on PSOC 6 CM4. I can read the ID and initialization seems to succeed but I cannot detect any tags.
Setup:
* I am using STEVAL-ST25R3916B reader expansion board with ST25R3916B.
* I have VBUS connected 5V, 3.3v to 3v3. SPI pins are properly connected and can read the ID. IRQ as +ve edge.
* I have attached spi transaction logs, I have the SPI bus connected to the logic analyzer in case if need any transaction through the logic analyzer.
* I have attached rfal_platform.h and have ST25R_COM_SINGLETXRX enabled and spi_transfer handles the SS pin.
Please let me know anything to try, not sure where to start.
Solved! Go to Solution.
2024-11-18 5:18 AM
Hi,
25MHz will not be possible with ST25R3916B. Please check the DS. Fortunately in your trace the SPI is rather at 1.6MHz.
Looking at the trace I find the IRQ pin staying high typically for ~6ms before getting cleared. The timeout handling is happening around <2ms but ISR seems to kick in only after 6ms.
Changing the timeouts is exactly just covering the underlying problems. The values should be fixed and are done in a way that they should pass if proper timer abstraction and interrupt handling is in place.
Regards, Ulysses
2024-11-19 1:53 PM
Hi @Ulysses HERNIOSUS
Thank you for all the help.
I have removed the RC filter on the GPIO lines, and I am now able to see the interrupts faster and detect tags.
Here is the working trace for anyone's reference.