cancel
Showing results for 
Search instead for 
Did you mean: 

Connect OAD OAD2 to st25ru3993 pin?

ROlss.3
Associate II
1 ACCEPTED SOLUTION

Accepted Solutions
Bart Herse
Senior II

Hello Robert,

by setting the msel bits you should be able to measure the Mixer DC level for I and Q. Please refer to STUHFL to see how we do the reflected power measurement in SW.

Let me know if this information was helpful.

Cheers,B

View solution in original post

2 REPLIES 2
ROlss.3
Associate II

ADC was forgotten.

Can we get any improved monitoring? Need to get RF level mixer with and without carrier also when ttags are not received. This for antenna tuning in setup with separate RX and TX paths. We see mixer i&q is zero with carrier. Correct values are seen when tags are received. Any insights?

Thanks

Robert

Bart Herse
Senior II

Hello Robert,

by setting the msel bits you should be able to measure the Mixer DC level for I and Q. Please refer to STUHFL to see how we do the reflected power measurement in SW.

Let me know if this information was helpful.

Cheers,B