2019-12-10 04:51 AM
The recommended voltage range is 85 volts which is also the same as the recommended voltage for the POWERSTEP01 device.
Why max Voltage 50V on IHM03A1 development board?
Solved! Go to Solution.
2021-01-12 02:19 AM
Hi @dungeonlords789,
the STM32 Nucleo Expansion boards for safety reason is limited to max 50 V of power supply.
2021-01-06 10:21 AM
The same question
@Cristiana SCARAMEL
2021-01-06 10:35 AM
Maybe security issues? Higher voltages need protection from touching.
2021-01-12 02:19 AM
Hi @dungeonlords789,
the STM32 Nucleo Expansion boards for safety reason is limited to max 50 V of power supply.