2024-12-09 03:52 AM - last edited on 2024-12-09 06:04 AM by mƎALLEm
The description of the on and off pins is not complete.
What happens if both are active at the same time?
Does one pin have higher priority than the other?
Is it possible to turn the device on/off just using one of the pins letting the other one unconnected?
Is the signal latched (after debounce time)?
2024-12-10 01:36 PM
Hope that helps?
Regards
/Peter
2024-12-12 06:10 AM
Hi Peter,
ok, I think I can manage with that description.
What happens when the Viper0P is first powered (VCC > VCC startup)?
Will it start switching in active mode or startup in ZPM mode and wait for an ON signal?
Thomas
2024-12-12 07:10 AM
When switching on, the VIPer0P always starts in normal operating mode, i.e. it can then be switched off with OFF. This behavior is described in the data sheet in section 5.11:
[..] If the device is disconnected from the mains or there is a mains interruption while in ZPM, the information in the logic is lost. When the input source is applied again, the IC will be restarted in normal mode. [...]
Hope that helps?
Regards
/Peter
2024-12-12 08:00 AM
Embarrassing, how did I not see that. Thank you for your response.
I think I have enough for deciding that I can actually use this device, which is great.
For the actual design though, I have not found anything about calculating the compensation network components?
Thomas
2024-12-12 08:31 AM - edited 2024-12-12 08:32 AM
You can simulate your design in the free-of-charge on-line simulator eDesignSuite, which also provides the compensation components.
Regards
/Peter