2022-10-05 03:33 AM
Hello,
I have an IPM10F and try to switch on the gate, so I can measure a current on the Output U. My Problem is I measure nothing.
I put a constant 3.3 Voltage to the Gate-Pin A-High. On the Output (U) I connect a resistance to override the LOW-Switch. After that I tried to measure with a multimeter. I linked one end to the resistance and the other to the ground, like normal.
Thank you
Solved! Go to Solution.
2022-11-08 04:50 AM
After a few researches, I found out, that the there is a bootstrap circuit. In that case you can't control the H-Side without first charging the Bootcapacitor.
Thank you and a have a nice day
2022-10-13 06:52 AM
Please provide the wiring diagram and the resistor value.
Thanks.
2022-10-13 07:54 AM
The first picture is the wiring diagram of the IGBT and the second from the STEVAL-IPM10F. I used 470k ohm resistors. After my question I tested the output by wiring three resistors 470k into a star connection and link them into the outputs (U,V,W). When I turned it on and put 400V, the oscilloscope showed how the voltage fall down, but with that current this should be impossible, so there is something wrong. Thank you!
2022-10-13 11:43 PM
Please use the first configuration, I mean the config. used in your first post, if you want to turn-on the High-Side Switch (or the Low-Side).
If you want to test the High Side switch:
If you want to test the Low-Side switch, use the same config as above but this time connect the resistor between U-OUT and P. For this test apply the input signal to the PWM-A-L input.
Hope this helps you.
2022-10-25 06:02 AM
I tried to test the High-Side switch with your points and it doesn't work. Is there a function in the IGBT, where I have to set the Low-side of high first before the High-side?
Thank you
2022-11-08 04:50 AM
After a few researches, I found out, that the there is a bootstrap circuit. In that case you can't control the H-Side without first charging the Bootcapacitor.
Thank you and a have a nice day