STWBC86 stops working after a few days
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-08 6:52 AM
Hi,
I have a array of 2x5 STWBC86 on a aluminium plate to make a charging station for multiple devices. They are all connected to a common 5V source and decoupled by a small filter of Ferrite bead and MLCC.
After testing them for a while i let them rest over the weekend with no devices sitting on the chargers.
After that only a few of the STWBC86 work correctly, the rest doesn't respond to devices. I connected WPStudio and found no errors to be shown but what i found is that the device has its power stage active all the time at its ping frequency.
Best regards
Stefan
- Labels:
-
STWBC86
-
Wireless charging
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-09 7:10 PM
Hi
About " i found is that the device has its power stage active all the time at its ping frequency".
Do you mean, STWBC86 is work on ping phase, even RX is on, it can not charging devices?
It will be nice if you can share below GUI picture to me to get more information.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-11 12:16 AM
Hi,
thanks for your fast reply.
Yes, RX is active, frequency is sitting at Ping frequency but no charging is happening.
I will have to let it rest over a few days to recreate the issue and take the screenshots.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-12 1:24 AM
Hi,
i could recreate it within a day.
Please find the screenshot below:
as well see a shot of the mode monitor:
RX and TX powers values are misleading in correlation to ICUR.
I also looked at the TX Interrupt latches and did find that if i write to "Did not occur" further testing does not alter them wich is different in a Controller not in that "error" state.
 
 
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-12 1:35 AM - edited ‎2024-04-12 1:37 AM
HI
From your picture, TX get cep timeout, which mean do not get RX Control error packet, So TX will cut off power.
Seems TX/RX communication is bad, What is RX output voltage? Do you use STWLC38-EVK for RX?
How about you adjust TX input voltage, set higher like 6V and try it.
Also you can use GUI and set "TX CE TO MAX" to 10, make cep timeout less to happened.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-12 1:42 AM - edited ‎2024-04-12 1:57 AM
Hi,
thanks for the swift reply.
i checked with a scope. the TX is still on (even if RX is removed). This will carry on forever until i reset the controller. Also i guess the CEP is there because of the removal of the RX on the previous charging cycle.
I use an IPhone for testing as well as Ti bq51050b. RX rectifier voltage is perfectly fine (5V) as well i checked the voltage at the VS pin of the TX. (DC-Level and AC component)
never the less will check with higher voltage.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-12 2:13 AM
Hi
Sorry I have mis-understand your issues.
Your issue is when RX remove, TX still in power transfer phase.
TX will get cep timeout and remove power Normally.
But your TX have some problem. So you need to modify set "TX CE TO MAX" to 0, make it easy to detect RX removed.
Please give me abnormal TX "TX EPT reason" GUI screenshort.
About clear latch intr, you need to use "TX interrupt Clear" in GUI.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-12 2:40 AM
Hi,
don't worry.
nearly got it. When i power up the TX everything runs as expexted. I can charge every kind of RX and place them and remove them very often without a problem.
My issue is that when i power up the TX and let it sit without a RX for one or two days, the Chip is showing the behaviour i showed above. Meaning that the TX has its powerstage on all the time even if it has never seen an RX ever.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-13 12:28 AM
Hi
I understand the issues now, i will do similar test to check.
TX default cfg is ping interval is 2sec, ping during is 80ms, So FW will do like this
1.ping 80 ms
2.Not find RX packet, sleep 2sec
3.Go to step1
Default TX CE To Max is 5, It means if ce timeout >5 it will go back to sleep,
So i think abnormal TX is detect CE packet and will not go to sleep.
So i suggest you set this value to 0 and test again.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-15 5:49 AM
Hi,
i will try and give you feedback asap.
the WPSTUDIO doesn't let me set 0 so i will try with the minimum which is 1.