cancel
Showing results for 
Search instead for 
Did you mean: 

STWBC86 stops working after a few days

S3rr4
Associate II

Hi,

I have a array of 2x5 STWBC86 on a aluminium plate to make a charging station for multiple devices. They are all connected to a common 5V source and decoupled by a small filter of Ferrite bead and MLCC.

After testing them for a while i let them rest over the weekend with no devices sitting on the chargers.

After that only a few of the STWBC86 work correctly, the rest doesn't respond to devices. I connected WPStudio and found no errors to be shown but what i found is that the device has its power stage active all the time at its ping frequency.

Best regards

Stefan

 

13 REPLIES 13

Hi 

I have check default cfg,

when TX detect three occasions.

  1. FOD
  2. OVP
  3. SYS ERR

It will disable re-ping, so TX will not ping. It need MCU/AP to clear this state and set command to "TX Start".

willzhou_0-1713233560206.png

willzhou_1-1713233609045.png

I have update new cfg and disable ept reason, please use this link cfg file

https://github.com/STwirelesscharger/STSW-WPSTUDIO/blob/main/STSW-WBC86FWBPP/STEVAL-WBC86TX_config_120D_BPP_NoEptReason.memh

After update this cfg file, GUI show all TX EPT Reping is disable.

willzhou_2-1713233710473.png

 

 

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
willzhou
ST Employee

Based on manual

https://www.st.com/resource/en/user_manual/um3161-getting-started-with-the-stevalwbc86tx-wireless-power-transmitter-evaluation-board-for-up-to-5-w-qibpp-applications-stmicroelectronics.pdf

It maybe tx stuck in fhop feature, change frequency and stay in power-stage mode.

willzhou_0-1713860670359.png

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi,

if i understand correctly Fhop is enabled by default.

so you reccomend to disable Fhop feature?

 

Best  regards

Stefan

yes, i recommend to disable  Fhop feature, attach is cfg for your test.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.