cancel
Showing results for 
Search instead for 
Did you mean: 

STWBC86 GPIO for LEDs

matt7
Associate

Hi,

When STWBC86 is operating fully independently without being interfaced with a host system, how can the GPIO be used to drive indicator LEDs to indicate charging status, fault etc? The datasheet shows how these can be programmed to inputs or outputs but how are the relevant functions assigned?

Cheers

1 ACCEPTED SOLUTION

Accepted Solutions
willzhou
ST Employee

Hi Jones

Yes, it can use, but different user will need different led, and special FW.

attach 1254 version is EVK board control LED example,

When TX is in charge mode LED will blink,

when rx remove, LED is on.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
willzhou
ST Employee

Hi Jones

Yes, it can use, but different user will need different led, and special FW.

attach 1254 version is EVK board control LED example,

When TX is in charge mode LED will blink,

when rx remove, LED is on.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.