2024-05-22 06:49 AM
Hi,
When STWBC86 is operating fully independently without being interfaced with a host system, how can the GPIO be used to drive indicator LEDs to indicate charging status, fault etc? The datasheet shows how these can be programmed to inputs or outputs but how are the relevant functions assigned?
Cheers
Solved! Go to Solution.
2024-05-22 07:54 AM
Hi Jones
Yes, it can use, but different user will need different led, and special FW.
attach 1254 version is EVK board control LED example,
When TX is in charge mode LED will blink,
when rx remove, LED is on.
2024-05-22 07:54 AM
Hi Jones
Yes, it can use, but different user will need different led, and special FW.
attach 1254 version is EVK board control LED example,
When TX is in charge mode LED will blink,
when rx remove, LED is on.