cancel
Showing results for 
Search instead for 
Did you mean: 

STSPIN32G4

AKINI.1
Associate

Hello ,

We want to drive two independent hub motor ( as like hoverboard) with STSPIN32G4 . Product overview says "Finally, with an additional external three-phase driver (such as the STDRIVE101) two independent 3-phase BLDC motors can be efficiently driven from the STSPIN32G4, offering an unprecedented BOM saving and application optimization." but I couldnt find any document .

Do you have any advice about that

Thank you

Abdullah KINIK

SAHA Robotik

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KnarfB
Principal III

Have you seen EVSPIN32G4, EVALSTDRIVE101?

hth

KnarfB

cedric H
ST Employee

Hello,

Dual drive is doable with the STSPIN32G4, but this solution is not yet supported by the X-CUBE-MCSDK . If you plan to use the ST firmware solution, the dual drive is planned to be back with the summer release 2023 expected begining of July.

Regards

Cedric