2023-01-02 04:27 AM
Hello ,
We want to drive two independent hub motor ( as like hoverboard) with STSPIN32G4 . Product overview says "Finally, with an additional external three-phase driver (such as the STDRIVE101) two independent 3-phase BLDC motors can be efficiently driven from the STSPIN32G4, offering an unprecedented BOM saving and application optimization." but I couldnt find any document .
Do you have any advice about that
Thank you
Abdullah KINIK
SAHA Robotik
2023-01-03 10:18 AM
Have you seen EVSPIN32G4, EVALSTDRIVE101?
hth
KnarfB
2023-01-03 12:18 PM
Hello,
Dual drive is doable with the STSPIN32G4, but this solution is not yet supported by the X-CUBE-MCSDK . If you plan to use the ST firmware solution, the dual drive is planned to be back with the summer release 2023 expected begining of July.
Regards
Cedric