2025-08-07 8:29 AM
[PN]: STSPIN32G4
[VERSION]: 6.4.0
[TOOL]: Motor Control Workbench
[DETAILS]:In this design, the second motor does not work as the interrupts that invoke the FOC_HighFrequencyTask by setting the motor ID into the array FOC_array[] are not enabled (TSK_DualDriveFIFOUpdate() is never called). Motor 1 happens to work as it's ID is 0 and the array is 0 initialised. Also the task TSK_HighFrequencyTask is only invoked at the PWM rate, not twice the PWM rate as it should be called once per motor, ie twice the PWM rate..
[EXPECTED BEHAVIOR]: The motor 2 current should be modulated but stays at 0 as the FOC_HighFrequencyTask(M2) is never called.
[HOW TO REPRODUCE]: just start motor 2 from motor pilot
Solved! Go to Solution.
2025-08-11 12:13 AM
Hello @GSB,
Each motor must be connected to a different ADC.
You can refer to the genuine EVSPIN32G4-DUAL board, which is a dual 1Shunt topology design.
2025-08-08 1:21 AM
Hello @GSB,
Thank you for your report.
Unfortunately, the dual drive, dual single-shunt, and single ADC use case is not covered in our current MCSDK release. We will add a restriction message in the release note to inform users of this limitation.
In our current implementation, two different ADCs are required for each drive.
2025-08-08 1:05 PM
2025-08-11 12:13 AM
Hello @GSB,
Each motor must be connected to a different ADC.
You can refer to the genuine EVSPIN32G4-DUAL board, which is a dual 1Shunt topology design.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.