cancel
Showing results for 
Search instead for 
Did you mean: 

STPM801 - unknown pins?

JTo
Visitor

Hello,

We are evaluating the STEVAL-STPM801 board, testing the STPM801 as integrated hot swap, soft start and oring protections device.

On the EVAL board the TM pins with nrs: 8, 13, 14, 27, 28, 29 are equipped with jumpers to select pull-up or pull-down, while in the datasheet of the STPM801 those pins must be connected to GND.

Also in the datasheet there is in chapter 5.1.5 STAND-BY mode enter/exit, in several graphs a pattern given for ENABLE-IN. I can not find the ENABLE pin.

 

However, on the EVAL board the signal connected to pin nr 8 in that figure 1 has the name TM_EN_1/2.

The TM lines are also feed to a jumper (e.g. JP17) with signal names like SPI1_*.

 

The difference between the Eval board and the datasheet makes it confusing.

  • Which pin is the Enable pin (mentioned in chapter 5.1.5 of the STPM801 datasheet)?
  • What is the functionality of the other TM pins?
  • Is there a "hidden feature" in the STPM801 available?

 

Hope that anyone can clarify.

kind regards

0 REPLIES 0