‎2020-04-15 05:18 PM
Hi,
I have a STEVAL-STSPIN3202 evaluation board and trying to setup the environment on MacOS. When I plug in the eval board with a USB B cable to my MacBook, I don’t see a device in both ls /dev/tty* and ls /dev/cu*
No devices even when I do, ioreg -p IOUSB
PortableA2-2:AllPlatforms jaimeyu$ ioreg -p IOUSB
+-o Root <class IORegistryEntry, id 0x100000100, retain 15>
+-o AppleUSBXHCI Root Hub Simulation@14000000 <class AppleUSBRootHubDevice, id 0x100000313, registered, matched, active, busy 0 (10 ms), retain 78>
+-o BRCM20702 Hub@14300000 <class AppleUSBDevice, id 0x100030b17, registered, matched, active, busy 0 (2 ms), retain 25>
| +-o Bluetooth USB Host Controller@14330000 <class AppleUSBDevice, id 0x100030b75, registered, matched, active, busy 0 (2 ms), retain 30>
+-o Apple Internal Keyboard / Trackpad@14400000 <class AppleUSBDevice, id 0x100030b2a, registered, matched, active, busy 0 (16 ms), retain 28>
I also tried downloading the STLINK upgrade found here. https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-programmers/stsw-link007.html
Ran it with ‘java -jar STLinkUpgrade.jar’ but I don’t see any devices under the list of devices. Screenshot attached.
I also have stlink installed with home-brew (brew install stlink)
On the eval board LD1 is blinking RED. Kindly help me debug this issue as I want to setup my dev environment on my MacBook.
Thanks,
VImal
Solved! Go to Solution.
‎2020-04-16 02:25 AM
Did you power the board before connecting to the MacBook?
The right sequence is:
1 apply the VM power supply to STEVAL-STSPIN3202 (J2 connector, the DL1 (red) LED turns on)
2 Connect the board to the PC through the USB cable
You can find more details on the STEVAL-STSPIN3202 in user manual UM2278
‎2020-04-16 02:25 AM
Did you power the board before connecting to the MacBook?
The right sequence is:
1 apply the VM power supply to STEVAL-STSPIN3202 (J2 connector, the DL1 (red) LED turns on)
2 Connect the board to the PC through the USB cable
You can find more details on the STEVAL-STSPIN3202 in user manual UM2278
‎2020-04-16 06:37 AM
That was it! Thanks a lot, Cristiana
I have another question regarding environment setup on mac.
20:25:45 **** Build of configuration Debug for project STSPIN32F0_Potentiometer ****
make all
User/subdir.mk:23: *** target pattern contains no `%'. Stop.
20:25:45 Build Finished (took 133ms)
The corresponding line on subdir.mk (generated file)
User/main_32F0.o: /Applications/STM32CubeIDE.app/Contents/MacOS/C:/GITshared/Cube/Stspin32f0_6steps_v1/stm32_cube/Projects/Multi/Examples/MotionControl/STEVAL-SPIN3202/Src/main_32F0.c
@echo 'Building file: $<'
@echo 'Invoking: MCU GCC Compiler'
arm-none-eabi-gcc -mthumb -mfloat-abi=soft -O0 -g3 -Wall -fmessage-length=0 -ffunction-sections -c -MMD -MP -MF"$(@:%.o=%.d)" -MT"$@" -o "$@" "$<"
@echo 'Finished building: $<'
@echo ' '
Let me know if I have to close this and take this topic to a different forum. Appreciate your help
‎2020-04-17 01:39 AM
My suggestion is to open a new post to address this programming problem (as you already made 😉 )