cancel
Showing results for 
Search instead for 
Did you mean: 

Steval -SPIN3201

oleg_sidorovich_1981
Associate II

Can I connect oscillograph to Steval -SPIN3201 for measurement currents of the phase? Where is this point on board?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Yes, of course.

Please take a look at the circuit diagrams and the UM2154 user manual of the STEVAL-SPIN3201. Perhaps you will find the shunt connections SENSE1P, SENSE2P and SENSE3P, which are amplified and then fed into the control at PA3/4/5. And if you then look at the board, you will find these test pads with a metal ring and the label PA3/4/5 around the controller.

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Yes, of course.

Please take a look at the circuit diagrams and the UM2154 user manual of the STEVAL-SPIN3201. Perhaps you will find the shunt connections SENSE1P, SENSE2P and SENSE3P, which are amplified and then fed into the control at PA3/4/5. And if you then look at the board, you will find these test pads with a metal ring and the label PA3/4/5 around the controller.

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
oleg_sidorovich_1981
Associate II

How I can use STEVAL-SPIN3201 for BLDC with MotorControl Workbench? In MotorControl Workbench only two types motors? To choose SM PMSM?

Hello @oleg_sidorovich_1981​ 

please if @Peter BENSCH​ answered your main question "Select as Best" his reply.

Moreover, to help the Community to easily find the answer to similar questions open a new topic with the second request.

If you feel a post has answered your question, please click "Accept as Solution"