2020-10-30 12:56 AM
Which debugger/programmer is recommended for STEVAL-HKI001V2 ?
2020-11-02 2:03 AM
Hello @Tore Kallevik welcome to the ST Community.
In the STEVAL-HKI001V2 user manual UM2645 in the section relating to ST Motor Control Workbench (page 9),
is suggested the connection with STLINK/V2 in-circuit debugger/programmer.
Let me know if I solved your doubts, if yes please "Select as Best".
2020-11-02 8:28 AM
OK, but I have now already purchased the STLINK-V3SET.
Will report back when I've received and tested it.
2020-11-03 1:50 AM
Ok @Tore Kallevik,
the several ST-LINK coexisting versions result from the incremental addition of new functionalities over time.
The STLINK-V3SET is the most recent and powerful ST-LINK generation.
We wait for your feedback when you get the new STLINK, thanks!