cancel
Showing results for 
Search instead for 
Did you mean: 

No connection to STEVAL-PCC009V2

stroggi11
Associate
Posted on February 24, 2014 at 20:34

Hi everybody,

I'm trying to get the EVAL6470H working, but the problems are begining at the STEVAL-PCC009V2. I can't get any connection via the ''dSPIN Evaluation Tool'' to configure the L6470.

I reflashed the firmware of the STEVAL-PCC009V2 several times as descibed in UM1612, but it still does not connect as ''STM32 based IBU UI Tool'' (see UM0935 page 15).

Can anybody help me to find a solution for this problem.

Sincerely,

Michael

#steval-pcc009v2 #eval6470h #l6470
2 REPLIES 2
mcl198
Associate
Posted on February 26, 2014 at 20:48

I have the same problem and sent in numerous support request. No reply. We called

our vendor today to see if they can get the issue resolved. Will let you know what

the vendor finds out.
Enrico Poli
ST Employee
Posted on March 06, 2014 at 08:39

Dears,

the last version of the PCC009V2 is connected to the PC as an HID device-

Moreover the dSPIN evaluation tool is obsolete, you need to use the SPINFamily evaluation tool instead (you can find it in the L6470 product page).

Regards

Enrico