2014-02-24 11:34 AM
Hi everybody,
I'm trying to get the EVAL6470H working, but the problems are begining at the STEVAL-PCC009V2. I can't get any connection via the ''dSPIN Evaluation Tool'' to configure the L6470.I reflashed the firmware of the STEVAL-PCC009V2 several times as descibed in UM1612, but it still does not connect as ''STM32 based IBU UI Tool'' (see UM0935 page 15).Can anybody help me to find a solution for this problem.Sincerely,Michael #steval-pcc009v2 #eval6470h #l64702014-02-26 11:48 AM
2014-03-05 11:39 PM
Dears,
the last version of the PCC009V2 is connected to the PC as an HID device- Moreover the dSPIN evaluation tool is obsolete, you need to use the SPINFamily evaluation tool instead (you can find it in the L6470 product page). Regards Enrico