2020-11-19 3:08 AM
I am working on BMS type of system that will recondition, balance, and maintain NiMH HEV batteries. I'm considering to use L9963 IC and its accompanying evaluation board EVAL-L9963 for my prototype. My system consists of nickel-metal hydride battery with 14 battery blocks connected in series with each block at 14.4 V nominal voltage(total nominal battery pack voltage about 202V) as shown in the figure below.
2020-11-19 4:37 AM
The website of the L9963 mentiones the measurement range per cell (per tap), so your 14.4V is way outside the limits:
16-bit voltage measurement with maximum error of ±2 mV in the [1.7 – 4.7] V range, in whole operating temp range
When your question is answered, please close this topic by choosing Select as Best.
/Peter
2020-11-27 2:01 AM
Hello @VVasy.1 welcome to the ST Community.
Does Peter’s explanation answer your question? If so, please "Select as Best" button in its reply.