2017-08-09 4:28 PM
Sorry if this is a simple question; I'm new to motor control.
I have the STEVAL-PCC009V2 and four EVAL6470Hs. I would like to drive them all at the same time. I saw in the user manual that you can't do that in the GUI, since it can only send one command to one device at a time. Is there an alternative method to do this? Perhaps through the script editor?
Thanks!
#dspin-family-firmware-library #eval6470h #pcc009v2-eval6470h-spinfamily #l6470h-discovery-eval6470-disk #discovery-eval6470-disc #dspin-gui #pcc009v22017-08-09 5:03 PM
Short answer yes.
Long answer is more complicated.
You will have to write your own code or script, but the move commands are non blocking. Meaning you can send one move command after another in very short order. You then monitor all four motor status's to decide when your moves are done.
I would refer to:
I have done something similar using the IHM02A1 attached to a Nucleo board (you just have to write a bunch of C code and use STM's libraries).
2018-02-09 12:31 AM
Please refer to
for details on communication protocol and how to implement a daisy chain architecture allowing the MCU to drive multiple devices with a single SPI interface.