2020-11-19 12:03 PM
Hi,
I am trying to use a STEVAL_PCC009V2 board connected to a EVAL6474H board to drive a stepper motor.
When I run the SPIN eval software I get a notice that the firmware is not the latest and I need to update it. I just ordered the board, but it shows as FW0.0. I have a ST-Link/V2 to program with, so I downloaded the IBUUI Board Updater, but it fails when I start the program with an error installing IBUUI.inf driver and exits.
I need to get this up and running ASAP so I can use it to move a stepper motor to evaluate the L6474.
Solved! Go to Solution.
2020-11-23 2:32 AM
Hello @DSabo,
you can find all the info for the manual update using the ST-LINK/V2 programmer in the documentation of SPINFamily Evaluation Tool.
In the user manual UM2022 (Appendix A at page 80):
the firmware can be updated
using the ST-LINK/V2 programmer or an equivalent tool.
Let me know if you were able to make the update successfully, if so please "Select as Best" button.
2020-11-23 2:32 AM
Hello @DSabo,
you can find all the info for the manual update using the ST-LINK/V2 programmer in the documentation of SPINFamily Evaluation Tool.
In the user manual UM2022 (Appendix A at page 80):
the firmware can be updated
using the ST-LINK/V2 programmer or an equivalent tool.
Let me know if you were able to make the update successfully, if so please "Select as Best" button.