cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I want to protect(over v and i) a 2.5hp AC motor with stm8 and BTA41 triac. I need to prevent triac to turn off when motor is in the off state because a light load series with motor, which control the water pressure and turns the motor on and off.

pghal.1
Associate

BTA41 has holding current of 80mA. Thank you all.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0